Input action: Change Shown Visualization Permalink

Table 837: Zoom to visualization

Visualization that is shown at the user input

“Assign”

Visualization that is selected from all available visualizations in the project or libraries.

Example: ‎visMain‎

“Assign expression”

Variable (‎STRING‎) that contains the name of the visualization

Example: ‎PLC_PRG.strVisu‎ for the following application code: ‎strVisu: STRING := 'visMain';‎

The order in which visualizations are displayed by user inputs is saved internally. The following options use this information.

“Previous shown visualization”

_cds_icon_option_activated_copy.png: Visualization that has already been shown before the current one

Requirement: A visualization switch has already occurred.

“Next shown visualization”

_cds_icon_option_activated_copy.png: Visualization that is next in the call order after the current one

Requirement: A visualization switch has already occurred which was called by “Previous shown visualization”.